Swagelok Products in Compliance with the Material Restrictions of European Directive 2015/863/EU
Swagelok Products in Compliance with the Material Restrictions of European Directive 2015/863/EU
Effected to Product: Products in table listed below
If you require product compliance with the material restrictions of the RoHS Directive from the following table, process sheet PS-59085 will need to be specified during the quote process, by adding “-59085” to the part number. This special designator was created to temporarily provide customers that require product that meet the material requirements in the RoHS directive.
We will advise when this process sheet is no longer needed. Product ordered to the process sheet will be marked as standard, without the special designator; however, package labeling will include the special designator in the part number. In addition, certifications requested while the process sheet is in use for these products will state the part number with the special designator; however, the reference field will state the part number without the special designator.
For more information, please contact our sales engineer if there is any questions or inquiries.